For the effective sealing of holes in fluid systems
New from norelem: Steel or stainless steel sealings plug
Producers of hydraulic or pneumatic units are familiar with this: When manufacturing the systems, auxiliary holes may need to be drilled in order to provide all the necessary channels. However, these should then be tightly resealed – especially given the extreme pressures that can occur in the units. Component specialist norelem now offers reliable sealing plugs for this purpose.
For hydraulic or pneumatic units to function properly, they must be closed units without any drop in pressure. During production, however, it is often necessary to drill auxiliary holes in order to provide all the required channels. If the systems are to function properly, it is essential that these holes are resealed to prevent pressure loss. For this purpose, norelem now offers a wide range of reliable sealing plugs.